Chat with us, powered by LiveChat

How can Victaulic Products Help HDPE Pipe Beat the Heat?

Victaulic Refuse-to-Fuse™ mechanical joints designed & tested to withstand pipe movement caused by temperature fluctuations

How can Victaulic Products Help HDPE Pipe Beat the Heat?

Last Updated on October 08, 2018
Originally Posted on February 23, 2018

With the humid, rainy season quickly approaching in North Queensland, Australian temperatures will soon soar well past 50◦C/120◦F and our focus turns to addressing the question “how will we beat the heat?” These extreme conditions call for creative solutions. While a lucky few can wait out the sweltering days in air conditioning, those who brave the elements (and the flies) resort to more traditional methods of keeping themselves cool.

HDPE Pipe
The cork hat is a ubiquitous weapon against the war on flies in Australia’s Outback. Corks dangling from a bucket hat swat flies away from your face, while the wide brim protects you from the elements.

Extreme weather can make people adopt some pretty funny behavior, and the same is true for piping systems. Did you know that the extreme temperatures like those experienced in North Queensland make HDPE pipe 10 times more susceptible to thermal expansion and contraction than steel? As the mercury moves, so does the pipe. Butt welded HDPE joints that are not done by-the-book are likely to pull apart under these conditions, the results of which can be catastrophic.

Previously failed joints at Glencore’s Oaky Creek Mine caused shut-downs, delays and headaches for the site. That is why in 2017 when the coal mine was set to install an 8km, 400mm OD HDPE raw water pipeline – a critical line that transports process water from the mine to the reverse osmosis plant, Glencore chose a new pipe joining method to help their HDPE pipeline beat the heat.

Victaulic Solutions for HDPE Pipe

Beat the Heat of Weather Conditions

Victaulic mechanical joints for HDPE pipe are designed and tested to withstand movement caused by temperature fluctuations which made it the ideal solution at the Australian mine. In fact, months after installation, Glencore reported a 100% joint success rate and zero leaks after the system was commissioned. Installing the pipeline was also a breeze. Victaulic joints are installed rain or shine, cold or hot. It doesn’t matter the weather condition, the installation process is the same.

 

Beat the Heat of Butt Welding

Even in the most ideal conditions, butt welding HDPE pipe is a temperamental process. Specialist poly-welders and pristine environmental conditions, void of any wind, rain or debris, are needed to ensure the joints are fused correctly. This is particularly critical for large-diameter HDPE pipelines, like the one at Oaky Creek. While additional equipment such as screens and tents can be used to protect the installation site, there is no guarantee (and no way to test) that a joint is properly fused. Victaulic mechanical joints eliminated all of these concerns for Glencore.

 

Beat the Heat of Project Schedules

The crew at Glencore was able to completely install each 400mm Victaulic joint in just 10 minutes, resulting in an overall time savings of 55%. Installation dropped from an estimated 80 days to only 35 days. And you really can’t beat those numbers.

Victaulic(唯特利)

Victaulic(唯特利)

Victaulic is the leading producer of mechanical pipe joining solutions. Engineered with confidence, our solutions put people to work faster, while increasing safety, ensuring reliability and maximizing efficiency.

Related posts

landfill

Fusion-Free Solution for Methane Mountain Modification

On a recent landfill methane pipeline project owners chose Victaulic's system solution for HDPE pipe to ensure a faster and safer installation proc...

Close up view of the glass bulbs with sand running through of an egg timer or hourglass measuring passing time counting down to a deadline

DEBUNKING MYTHS ABOUT JOINING HDPE: MYTH #3 – FUSION IS FASTER

The traditional method of joining HDPE pipe is with fusion, however this process can be negatively affected by many variables. If you are looking f...

Arms holding weights - represents strength of Victaulic HDPE pipe fittings for joining HDPE pipe

澄清有关连接高密度聚乙烯(HDPE)管道的误解:第2个误解—熔接接头强度更高

Victaulic's system solution for HDPE pipe is designed with strength & durability in mind. Under extreme pressure tests, Victaulic mechanical joints...

Recent posts

Engineers Week, September 18, 2013, Cat with Anya and Olga

Four Ways to Inspire Wonder for Engineers Week

As February 17-23 celebrates National Engineers Week. Victaulic is proud to bring our expertise to future STEM professionals and inspire wonder in ...

2019 The Increase in Cold Storage

Have you ever wondered where your temperature-controlled medicine is stored? Or where your groceries were stored before you purchased them online? ...

Man (from neck to thighs) wearing suit with white cogs & wheels super imposed over him; that image is super imposed over a construciton project

Preconstruction Software Integration: The fuel powering construction productivity

As we enter into 2019 the focus is on the integration of preconstruction software, and how this powerful data is driving construction productivity....